Links Where to Buy Home
Hardware
 

RoadRelay 4 Hardware

Why won't my RoadRelay 4 display turn on?

The RoadRelay 4 is probably not getting power. Check that the key is in the "On" position, no fuses are blown, and the wiring is consistent with what is specified in the installation manual. Verify with a voltmeter that power is being applied from the 6-pin vehicle connector pins to the RoadRelay 4. Press the "Up" arrow several times to brighten the display.

Why isn't my RoadRelay 4 reading any data and I am getting either a "RoadRelay Data Link Failure" or "Improper Data Link Connection" error message?

It is likely that the one or more of the data link connections has come loose. Verify that all the data link wires and splices are tightly connected, as specified in the installation manual, the key is in the "On" position, and there are no open or shorted wires and no bent connector pins. Measure the data link wires with a voltmeter to ensure they are in the voltage range specified in the troubleshooting section of the installation manual.

What should I do if I see a "No Power From Backup Battery" error message?

It is likely that either the loop-back connector is not installed or the back-up battery is dead. Make sure that the 10-pin loop-back connector has been properly installed, as described in the installation manual. Measure the back-up battery voltage on the 10-pin loop-back interface connector on the RoadRelay 4 to verify it is not below 2.0 Volts DC. If the battery is dead, you will need to have it replaced at an authorized Cummins repair facility.

What should I do if I see a "RoadRelay Failure" error message?

Take your failed RoadRelay 4 unit to an authorized Cummins repair facility.

 

© 2009 Cummins Inc.